2018-08-02 5:23 PM
I have installed STM32CubeMX version 4.26.1. I have downloaded X-CUBE-MEMS1 5.0.0. I go to Help->Manage embedded software packages, and click on "From Local..." I pick the zip file containing X-CUBE-MEMS1, and I get the error message "This Package version is not managed on this version of STM32CubeMX".
How can I use X-CUBE-MEMS1 to generate BSP code to interact with the IKS01A2 expansion board that I purchased? I am using a STM32L476RGT6.
2018-08-02 7:26 PM
X-CUBE libraries don't integrate with CubeMX, they are stand-alone code examples
2018-08-03 11:27 AM
Ah. So there's no way to use the CubeMX software to generate code that will initialize and talk to an expansion board? (In this case the IKS01A2 MEMS board...)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.