2024-04-22 8:42 AM
Hello to support-team and specialists,
We have the demo-board: NUCLEO-B071RB / MB1360-G071RB-C02
and want to work the Demo-Example: "Hello World" with:
X-Cube-Display: X-NUCLEO-GFX01M2.
We loaded the latest STM32CubeMX: Version: 6.11.0
Configuring the Software-Packs will list the following Warning/Error: "
This version is not compatible with the current version of STM32CubeMX.
It is compatibel with STM32CubeMX from 6.7.0 up to 6.8.1 !!!
Is there a workaround?
Could the team for the expansion-boards fix the version update?
Any help will be appreciated.
Thank you in advance.
Armin
2024-04-22 9:41 AM
Hello @RWM_KHE_1 and welcome to the ST Community :smiling_face_with_smiling_eyes:.
If you want to use this package, You should use one of the mentionned version of CubeMX.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.