2022-08-24 2:45 AM
In adc.c (HAL driver), line 89 there are wrong constants generated:
LL_ADC_SetCommonPathInternalCh(__LL_ADC_COMMON_INSTANCE(ADC1), LL_ADC_PATH_VREFINT|LL_ADC_PATH_TEMPSENSOR);
correct is:
LL_ADC_SetCommonPathInternalCh(__LL_ADC_COMMON_INSTANCE(ADC1), LL_ADC_PATH_INTERNAL_VREFINT|LL_ADC_PATH_INTERNAL_TEMPSENSOR);
Solved! Go to Solution.
2022-08-25 4:26 AM
Hi @straubm ,
Thanks for sharing the details.
It is simple and you were able to fix it manually, but it needs to be fixed at STM32CubeMX side.
Internal ticket was submitted to keep track of the issue.
Internal ticket number: 133589 (This is an internal tracking number and is not accessible or usable by customers).
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-08-24 3:57 AM
Hi @straubm ,
Which STM32 product are you using please, or STM32Cube FW package?
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-08-24 4:57 AM
Hi Amel,
OMG, I forgot that crucial info.
CubeMX and STM32L4(1.17.2).
Btw, no big deal, I fixed it manually.
2022-08-25 4:26 AM
Hi @straubm ,
Thanks for sharing the details.
It is simple and you were able to fix it manually, but it needs to be fixed at STM32CubeMX side.
Internal ticket was submitted to keep track of the issue.
Internal ticket number: 133589 (This is an internal tracking number and is not accessible or usable by customers).
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-08-25 5:13 AM
but it needs to be fixed at STM32CubeMX side.
That's why I reported it :D
Over and out.
Take care.
2022-11-28 8:24 AM
Hello @straubm
I want to inform you that the issue is fixed in the 6.7.0 CubeMX release available on the ST web site under this link.
Semer.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-11-28 8:50 AM
I followed the link and installed the MX 6.7.0 version. But the STM32CubeIDE still uses 6.6.1-RC2. How do I fix it?
2022-11-28 9:07 AM
Nevermind. It is in the STM32CubeIDE update 1.11.0. Thanks
2022-11-28 9:43 AM
Hello @Semer CHERNI,
thanks for fixing it and for the info.
Take care
Martin.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.