2023-12-27 8:51 AM
I want to generate an interrupt on the rising edge of PI0 on the M4 CPU.
Unfortunately, when I program the GPIO With ARM Cortex-M4 pin context assignment, the code generated is as follows in gpio.c:
EXTI_InitStruct.Line_0_31 = LL_EXTI_LINE_0;
EXTI_InitStruct.Line_32_63 = LL_EXTI_LINE_NONE;
EXTI_InitStruct.Line_64_95 = LL_EXTI_LINE_NONE;
EXTI_InitStruct.LineCommand = ENABLE;
EXTI_InitStruct.Mode = LL_EXTI_MODE_IT;
EXTI_InitStruct.Trigger = LL_EXTI_TRIGGER_RISING;
LL_EXTI_Init(&EXTI_InitStruct);and in stm32h7xx_it.c:
void EXTI0_IRQHandler(void)
{
...
if (LL_EXTI_IsActiveFlag_0_31(LL_EXTI_LINE_0) != RESET)
{
LL_EXTI_ClearFlag_0_31(LL_EXTI_LINE_0);
...But this is incorrect because while both init + IRQ executes on the M4, it programs the M7 interrupts delivery.
The correct way to make it work is to replace the following is the code above:
LL_EXTI_MODE_IT => LL_EXTI_MODE_C2_IT
LL_EXTI_IsActiveFlag_0_31() => LL_C2_EXTI_IsActiveFlag_0_31
LL_EXTI_ClearFlag_0_31 => LL_C2_EXTI_ClearFlag_0_31
Solved! Go to Solution.
2024-01-03 8:29 AM
Hello @cberg.1 ,
I escalated the problem to CubeMX team in an internal ticket (ID : 168700 ) to take a closer look at this issue.
(PS: ID 168700 is an internal tracking number and is not accessible or usable by customers).
Thanks.
Mahmoud.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-01-03 1:57 AM
Hello @cberg.1 ,
First let me thank you for posting and welcome to the ST Community.
Your request is under investigation, and I will get back to you ASAP.
Thanks.
Mahmoud.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-01-03 8:29 AM
Hello @cberg.1 ,
I escalated the problem to CubeMX team in an internal ticket (ID : 168700 ) to take a closer look at this issue.
(PS: ID 168700 is an internal tracking number and is not accessible or usable by customers).
Thanks.
Mahmoud.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-08-20 7:07 AM
I don't know the status of your internal bug, but I want to note that:
On version Version: 1.16.0 of STM32CubeIDE, I see that half the bug has been fixed.
Cedric
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.