2019-07-25 7:41 AM
Hello,
I am starting a project using STM32CubeMX v5.3.0 and looking at using the STM32H745ZI. If I set up the following options:
then I get a yellow exclamation warning on RCC and CRS SYNC is highlighted with the warning "CRS SYNC conflict with DEBUG Debug JTAG (5 pins) or/and USB Should be enabled".
Can I ignore this warning? I would have thought in this configuration, with CRS SYNC being sourced from LSE that I do not need the CRS SYNC pin which is shared with JTDO and no warning should be issued. Even with CRS SYNC disabled (although I do not see how that is achieved from the reference manual) the warning is still shown.
Or does STM32CubeMX just bundle up all the possible warnings, errors and remedies and display them, even if you have settings that would not cause the conflict? I can see in the CRS SYNC drop down that using the GPIO is invalid, but I've also tried enabling USB FS and HS and the warning message about enabling USB still persists.
Thanks.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.