2020-01-31 6:06 AM
screenshot from an .ioc file created with an earlier version of CubeMx
CubeMx version 5.30
screenshot from an .ioc file created with CUbeMx version 5.5.0
Full details of installation:
STM32CubeMX - STM32 Device Configuration Tool
Version: 5.5.0-RC6
Build: 20191220-1511 (UTC)
Copyright (c) 2018 STMicroelectronics. All rights reserved
STM32CubeIDE
Version: 1.2.1
Build: 5190_20200115_1224 (UTC)
(C) 2019 STMicroelectronics ALL RIGHTS RESERVED
Thanks
2020-01-31 6:09 AM
Hello @Sebastiain Fernandez ,
Issue has been fixed , the fix will be available in the next release.
Best Regards,
Khouloud
2020-01-31 6:16 AM
Thanks
Sorry if this question had been answered before I didn't find any conversations related to the issue
Best Regards
2020-01-31 6:18 AM
not problem you're always welcome
2020-01-31 6:46 AM
Hi I just found that the problem is in fact related to the STM32CubeH7 firmware package 1.6.0.
I downgraded to version 1.5.0 with CubeMx 5.5.0 and the ADC3 vbat, temp and vrefint channels are available
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.