2021-05-27 7:26 PM
I make a usbh freertoss programe by stm32cube.
The programe have three thread
/* definition and creation of defaultTask */
osThreadDef(defaultTask, StartDefaultTask, osPriorityNormal, 0, 512);
defaultTaskHandle = osThreadCreate(osThread(defaultTask), NULL);
/* definition and creation of commTask */
osThreadDef(commTask, StartCommTask, osPriorityIdle, 0, 512);
commTaskHandle = osThreadCreate(osThread(commTask), NULL);
/* definition and creation of LedTask */
osThreadDef(LedTask, StartLedTask03, osPriorityIdle, 0, 512);
LedTaskHandle = osThreadCreate(osThread(LedTask), NULL);
The usbH thread is created in StartDefaultTask thread.
#if (USBH_USE_OS == 1U)
#if (osCMSIS < 0x20000U)
/* Create USB Host Queue */
osMessageQDef(USBH_Queue, MSGQUEUE_OBJECTS, uint16_t);
phost->os_event = osMessageCreate(osMessageQ(USBH_Queue), NULL);
/* Create USB Host Task */
#if defined (USBH_PROCESS_STACK_SIZE)
osThreadDef(USBH_Thread, USBH_Process_OS, USBH_PROCESS_PRIO, 0U, USBH_PROCESS_STACK_SIZE);
#else
osThreadDef(USBH_Thread, USBH_Process_OS, USBH_PROCESS_PRIO, 0U, 8U * configMINIMAL_STACK_SIZE);
#endif /* defined (USBH_PROCESS_STACK_SIZE) */
phost->thread = osThreadCreate(osThread(USBH_Thread), phost);
#else
/* Create USB Host Queue */
phost->os_event = osMessageQueueNew(MSGQUEUE_OBJECTS, sizeof(uint32_t), NULL);
/* Create USB Host Task */
USBH_Thread_Atrr.name = "USBH_Queue";
#if defined (USBH_PROCESS_STACK_SIZE)
USBH_Thread_Atrr.stack_size = USBH_PROCESS_STACK_SIZE;
#else
USBH_Thread_Atrr.stack_size = (8U * configMINIMAL_STACK_SIZE);
#endif /* defined (USBH_PROCESS_STACK_SIZE) */
USBH_Thread_Atrr.priority = USBH_PROCESS_PRIO;
phost->thread = osThreadNew(USBH_Process_OS, phost, &USBH_Thread_Atrr);
#endif /* (osCMSIS < 0x20000U) */
#endif /* (USBH_USE_OS == 1U) */
But the function can not goto USBH_Process_OS.
I can see the UsbH thread is blocked when I use osThreadList;
2021-06-01 1:47 AM
UP UP UP UP
2021-07-05 7:04 PM
2021-07-13 7:50 AM
Hello @JYu.2 ,
Can you provide the firmware package used?
Thanks in advance.
BeST Regards,
Walid
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.