2019-09-17 12:33 AM
In the help document concerning .extSettings file the information is unclear.
As I read it the Groups section is supposed to create/add directories and files.
It does not. I have generated the project for SystemWorkbench and EWarm.
I downloaded a test version of IAR to verify. None of the directories or files are added as described.
The only change I can find is an entry in .mxproject file.
The specified file is added to SourceFiles in PreviousUsedSW4STM32Files section.
Can anybody explain how to use the Groups section.
2019-09-17 1:09 AM
Hi @Markus GIRDLAND do you have any insight on this. Nobody seems inclined to reply
2019-09-18 3:05 AM
I'm afraid I'm not much help here. I don't know a lot about MX/SW4STM32.
What documentation are you reading and where are you creating groups?
2019-09-18 3:26 AM
2019-09-18 3:41 AM
I believe you're better off speaking to an MX expert about that, such as @Nawres GHARBI .
Regarding the template files that is set to be fixed in the next version of CubeIDE.
2019-09-18 3:43 AM
2019-09-18 3:56 AM
Hi @Nawres GHARBI Do you have any insight in to this problem
2019-10-14 3:08 AM
Hello @davidregan9 ,
For IAR, it works fine , problem appears with SW4STM32.
This issue will be fixed in the next CubeMX release.
Best Regards,
Khouloud.
2020-01-07 3:03 AM
the .extsettings file can not create files and directories that do not exist but allows you to add additional settings witch can be used when external tools call STM32CubeMX to generate the project and require specific project settings.
Regards,
Khouloud.
2020-01-07 3:33 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.