2025-03-05 1:15 AM
Hello, I'm trying to implement a USBX host... and the code generates a lot of runtime errors. I assume everything is setup properly from CubeMX, but the code always fails.
1- I see that the mutex was created from the debug session: (ux_system_mutex)
2- the system fails when trying to initialize the UX system.
3- The error came from _ux_utility_mutex_on() and generates an error code 0x04
VOID _ux_utility_mutex_on(UX_MUTEX *mutex)
{
UINT status;
/* Call ThreadX to get system mutex. */
status = tx_mutex_get(mutex, TX_WAIT_FOREVER);
/* Check for status. */
if (status != UX_SUCCESS)
{
/* Error trap. */
_ux_system_error_handler(UX_SYSTEM_LEVEL_THREAD, UX_SYSTEM_CONTEXT_UTILITY, status);
}
/* Return to caller. */
return;
}so, it is trying to get the mutex (ux_system_mutex) and then wait forever....
4- If I look at the AzRTOS manual: 0x04
5- The base code was auto generated by CubeMX. So basically it is trying to initialize memory using a mutex before starting the threads....
6- to make matters worse, the error code (status) is not passed to the calling function properly, so it took a lot of time to find this problem, and the ux_error_handlers does absolutely nothing (ie no while(1))
Solved! Go to Solution.
2025-11-10 5:40 AM
Regarding the mutex operation is being called before threadX scheduler has started.
I got the confirmation, you need to avoid initializing USBX stack before starting the ThreadX. This is a known limitation in USBX.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-03-05 5:48 AM
Hi @matt-crc
Would you attach ioc file to reproduce?
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-03-05 8:44 AM
2025-03-05 10:42 PM
Hi @FBL
This is my first project with STM32, so I'm not too familiar on how ST works... so I have 3 questions:
1- How long does it usually take for ST to analyze and fix the problems reported (weeks, months, etc)? and how often do you release updates?
2- Do you know of a way to disable the auto-code generator from updating a particular file? (for example if I fix this problem in app_azure_rtos.c, I don't want CubeMx to update this file anymore.)
3- It would be really nice if CubeMX always added a user area at the very beginning of the file and a user area at the end of the file to all generated files, then users can disable the updating of a file. This would fix item #2 above. Can this be done for all your files? (example shown below)
/*User code begin - start of file */
/*User code end - start of file */
----
CubeMX code will be updated in this area
----
/* User code begin - end of file */
/* User code end - end of file */then our code would look like this:
/*User code begin - start of file */
#ifdef (USE_CUBEMX_CODE)
/*User code end - start of file */
----
CubeMX code will be updated in this area
----
/* User code begin - end of file */
#endif
----
User code will remain untouched here - for bug fixes and enhancements
----
/* User code end - end of file */
2025-03-06 6:07 AM
Hi @matt-crc
An internal ticket is submitted to dedicated team to fix initialization order in app_azure_rtos.c (204777)
Another ticket is submitted to Tools team to add user section at the end of app_azure_rtos.c file to make it more customizable (204781).
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-07-10 6:52 AM
Hi,
Any news on this matter? It's been 4 months, and I still see this bug in action. In fact, it has been reported like a year ago. https://community.st.com/t5/stm32cubemx-mcus/usbx-blocking-isr/td-p/698199
2025-11-10 5:40 AM
Regarding the mutex operation is being called before threadX scheduler has started.
I got the confirmation, you need to avoid initializing USBX stack before starting the ThreadX. This is a known limitation in USBX.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-11-10 9:02 AM
Hi @FBL
you're too funny... I guess you should inform your programmers because the base code was from your examples. Since it was 6 months ago, I don't remember which USBX H7 it was from, but I'm pretty sure they all do it.
Matt
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.