2020-04-14 9:09 PM
Hello to all,
I am having problems with the CDC USB Device application. Does some one have a working USB example for STM32L1? .
I am using latest version of CubeMx and STM32L1 firmware v1.9.0. The problem is that PC does not recognize the USB Device (Device unknow error 43).
I put together a very basic app, just to check if windows (W7 or W10) recognize the USB device but it fails.
I have been doing some HW and SW check and looks all fine but can't find the problem.
I would like to test a working USB example for STM32L1 or otherwise an older firware version just for testing.
Will be very grateful if I can get some help on this.
Thanks
2020-04-15 1:24 AM
Hello @Pmang.1 ,
Have a look to this FAQ: USB device not recognized, it may help you.
You can refer to the CDC example in the STM32CubeL1 firmware package and get inspired from the available one:
STM32Cube_FW_L1_V1.9.0\Projects\STM32L152D-EVAL\Applications\USB_Device\
Best Regards,
Imen
2020-04-15 8:32 AM
Try to swith the USB_DP & USB_DM pins.
USB DP & DM pins swapped would result in this.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.