2025-02-20 8:44 AM - edited 2025-11-11 4:42 AM
When trying to build an STM32CubeMX V6.13.0 generated cmake+gcc project with clang there are two files that generate errors:
sysmem.c produces the following error:
Core/Src/sysmem.c:30:35: error: use of undeclared identifier 'NULL'
[build] 30 | static uint8_t *__sbrk_heap_end = NULL;
This is caused by the fact that only errno.h and stdint.h are included. None of them officially define NULL. But they probably do in gcc. Also ptrdiff_t is undefined.
sysmem.c can easily be modified by either:
Linker script:
Linker scmemory region not defined: RAM
[build] >>> _estack = ORIGIN(RAM) + LENGTH(RAM); /* end of "RAM" Ram type memory */ript generates the following errors:
and
[build] ld.lld: error: STM32L431RCTX_FLASH_clang.ld:93: symbol not found: READONLY
[build] ld.lld: error: unable to place section .ARM.extab at file offset [0xFFFFFFFFF8010000, 0xFFFFFFFFF800FFFF]; check your linker script for overflows
Linker script can easily be modified by:
Modifying sysmem.c would have priority in my opinion since linker scripts often need to be modified anyway.
The resulting code now builds with both clang and gcc without errors (many warnings though, but that is kind of the point for me, so I can run clang-tidy and parse the syntax tree).
Solved! Go to Solution.
2025-11-11 2:41 AM - edited 2025-11-11 4:24 AM
@Semer CHERNI One question:
The name of the linker file was changed from stm32l476rgtx_flash.ld to STM32L476XX_FLASH.ld. Why was it changed? The reason I ask is that linker files frequently change names. This makes version control harder.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.