2019-01-28 10:11 PM
Am Working with STM32L4R9 Discovery Kit
2019-01-29 2:08 PM
Open the user manual https://www.st.com/content/ccc/resource/technical/document/user_manual/group0/ae/a3/af/94/27/d8/46/3f/DM00421316/files/DM00421316.pdf/jcr:content/translations/en.DM00421316.pdf
Page 53:
By default in this board, the USART is by default connected to STMod+
To have the SPI connected, the solder bridge 21 17 and 19 must be short.
Otherwise, a mux device is present according to the note in case soldering is to be avoided.
The solder bridges (SB) are available on PCB to select chosen Port, but they are not used by default: Instead of SB, an embedded SPDT quad switch is used to select Port. It is controlled by 2 GPIOs from the MFX_V3 Expander (STMOD+_SEL_0 and _1), please see Table 32 description below (Bold text is default configuration to support MikroBUS modules using MB1280 fan-out board)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.