2023-07-17 12:17 AM
Hi,
I am trying to integrate ETH & TFT LCD i nto my application using STm32H757 MCU
TFT LCD display interface is working properly unless ETH is configured
ETH is configured through below link
Ethernet module is able to get the IP address connected to DHCP server
MPU is configured and I-Cache & D-Cache Enabled as given in above link
One problem with ETH configuration is - Application is not executing in normal mode.
Need to click on F5 (3-5 times) in debug mode as in the below link'
When enabling D-Cache for ETH irrespective of MPU region configurations, TFT LCD is not displaying clearly
Disabling D-Cache makes LCD display clear
Unable to find the proper solution for both issues
Please extend your valuable support to fix it
2023-07-21 4:03 AM
Hello @NAham.1,
Would you please share your memory definitions in the linker file? Have you tried to increase the stack size?
When D-Cache is enabled, it can cause issues with memory coherency if the memory regions are not properly configured. Would you share your MPU configuration?
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.