2024-04-09 7:07 AM
My project was generated a few months ago (LWIP + FREERTOS on M7). The project was working without an issues. A few days ago I wanted to include CAN interface and after converting IOC to latest version, I have issue: LWIP was deactivated. I am not able to activate LWIP just for M7. LWIP can be activated M7 + M4. If I active LWIP on both cores, I am not able to use FREERTOS
Solved! Go to Solution.
2024-07-05 7:46 AM
Issue fixed in the latest version of CubeMx 6.12.0
2024-04-09 7:37 AM
Hello @LinasSt and welcome to the ST Community :smiling_face_with_smiling_eyes:.
I suggest you to refer to this FAQ and the examples available on this GitHub repository.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-04-09 7:48 AM - edited 2024-07-05 7:44 AM
Hello @LinasSt ,
I'm raising this behavior internally (Ticket 178614). I think it's a regression in CubeMx. I'll get back to you as soon as I have a feedback/confirmation.
Thank you.
2024-07-05 7:46 AM
Issue fixed in the latest version of CubeMx 6.12.0
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.