2021-06-01 4:17 AM
Does ST publish a roadmap of features/enhancements for CubeIDE? I'd really like to know what is planned for STM32CubeIDE for the dual core H7 chips.
For example, in Project Manager->Project, there is a setting "Dual Core Boot Mode", but it is greyed out. When will this be available? I'd like my CM4 to do boot initialization (for example of the RCC) rather than the CM7, but it seems this is not possible to generate out of CubeIDE right now.
2021-06-01 4:55 AM
Hello!
We don't have a public roadmap of planned features that we publish anywhere. This specific feature is currently not on the roadmap.
2021-06-01 4:58 AM
@Markus GIRDLAND So essentially, if you plan on using an H7 dual core chip, you can't count on using CubeIDE/MX at all. Only in the very narrow way ST currently has it set up. That is a bummer because CubeIDE/MX is so helpful in getting your HW setup correct. That's almost enough to discourage me from using the chip in a new design.
2021-06-01 1:52 PM
According @Markus GIRDLAND maybe no automation at that time but some doc may help you I guess.
Is option bytes may help you ?
See STM32H745/755 and STM32H747/757 lines dual-core architecture - Application note starting page 16
See full refman: https://www.st.com/resource/en/reference_manual/dm00176879-stm32h745-755-and-stm32h747-757-advanced-arm-based-32-bit-mcus-stmicroelectronics.pdf
2024-12-27 3:59 PM
And 3.58 years later, "Dual Core Boot Mode" is still greyed out .... :(
2024-12-30 10:37 AM
They've probably got the whole dev team working on hype-y AI features like all tech companies right now. Sigh.
2024-12-30 11:52 AM
Agreed.
Haven't we all learned the lessons from "hype-space cyberspace" ?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.