2021-08-19 2:35 AM
Bug:
CubeMX codegeneration for the RCC (clock module) may lead to hardfault during clock initialization.
I have a minimal example IOC (attached).
This faults during RCC initialization (in SystemClock_Config), after LL_RCC_SetSysClkSource(LL_RCC_SYS_CLKSOURCE_PLL1);
This happens because the peripheral domain prescalers need to be increased BEFORE switching to the faster clock (AFAICT), this would mean moving LL_RCC_SetSysClkSource(LL_RCC_SYS_CLKSOURCE_PLL1) toward the end of the function (after LL_RCC_SetAPB4Prescaler).
This is right now 100% reproducible for me, but I suspect that instruction prefetching can potentially hide/sidestep the problem: If I enable -Os optimization flags, then the problem vanishes depending on how many __NOP() instructions (0-3) are inserted directly before LL_RCC_SetSysClkSource(LL_RCC_SYS_CLKSOURCE_PLL1);.
Best way to reproduce the hardfault is single-instruction-stepping over this section with the debugger (that catches it every time for me).
Workaround:
Use HAL layer instead.
Occurred with STM32H730VBH in CubeMX v6.3.0, but I'd assume that other controllers and older CubeMX versions are also affected.
Solved! Go to Solution.
2021-08-23 6:03 AM
Hi again @Wolfgang Pupp ,
I have checked from my side, and I confirm the issue, you have right.
Sorry for any inconvenient that may have caused and thanks for raising this issue to our attention, it will be fixed.
Khouloud
2021-08-19 7:12 AM
Hello @Wolfgang Pupp ,
Thank you for your post,
I'll check it then I'll get back to you.
Khouloud
2021-08-23 6:03 AM
Hi again @Wolfgang Pupp ,
I have checked from my side, and I confirm the issue, you have right.
Sorry for any inconvenient that may have caused and thanks for raising this issue to our attention, it will be fixed.
Khouloud
2024-11-21 3:42 PM
This bug with the LL driver is still present - 3 years later...
I moved the lines of codes setting PLL as the source AFTER the Set---PreScalar calls, and the code works. Unfortunately this fix will be blown away the next time I generate code from CubeMX.
This is with the latest versions of everything as of 11-21-24 and using a H757 target. I guess I'll try the bloated HAL version. :(
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.