2024-02-13 1:05 PM
I'm using a STM32H563 Nucleo and the latest version of CubeMX along with the Keil (V6.19 C Compiler - uVision IDE V5.38)
I have discovered a weird issue where even though CubeMX seems to be generating the initialization code for the baud rate for UART9 correctly, it does not actually get loaded into the UART9 Baud Rate Register (BRR) using the Lower Level (LL) libraries:
UART_InitStruct.BaudRate = 19200;
UART_InitStruct.DataWidth = LL_USART_DATAWIDTH_9B;
UART_InitStruct.StopBits = LL_USART_STOPBITS_1;
UART_InitStruct.Parity = LL_USART_PARITY_ODD;
UART_InitStruct.TransferDirection = LL_USART_DIRECTION_TX_RX;
UART_InitStruct.HardwareFlowControl = LL_USART_HWCONTROL_NONE;
UART_InitStruct.OverSampling = LL_USART_OVERSAMPLING_16;
LL_USART_Init(UART9, &UART_InitStruct);
LL_USART_ConfigAsyncMode(UART9);
LL_USART_Enable(UART9);
When I compile and execute the code, the USART_BRR value stays unchanged at 0 hex. I have tried the same thing on UART7 and it works just fine. I am trying to trace through the LL code and see where it's failing to load the UART9 BRR, but in the meantime I thought it best to report the issue. The behavior is completely repeatable.
Solved! Go to Solution.
2024-02-13 11:38 PM - edited 2024-02-14 6:10 AM
Hello @MSilv
Thank you for having reported this. I've reproduced the issue, and I can confirm it.
I've escalated this issue for fix in the internal ticket number 173387.
(PS: Internal ticket number 173387 is not accessible or usable by customers).
Until that, you can still use the HAL driver for the UART9 or the LL driver with other UARTs.
Also, as a temporary workaround, you can use integrate this function to the MX_UART9_Init(void):
LL_USART_SetBaudRate(USART_TypeDef *USARTx, uint32_t PeriphClk, uint32_t PrescalerValue, uint32_t OverSampling,uint32_t BaudRate)
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-02-13 11:38 PM - edited 2024-02-14 6:10 AM
Hello @MSilv
Thank you for having reported this. I've reproduced the issue, and I can confirm it.
I've escalated this issue for fix in the internal ticket number 173387.
(PS: Internal ticket number 173387 is not accessible or usable by customers).
Until that, you can still use the HAL driver for the UART9 or the LL driver with other UARTs.
Also, as a temporary workaround, you can use integrate this function to the MX_UART9_Init(void):
LL_USART_SetBaudRate(USART_TypeDef *USARTx, uint32_t PeriphClk, uint32_t PrescalerValue, uint32_t OverSampling,uint32_t BaudRate)
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.