2016-10-08 9:30 PM
BOARD for STM32F303RET6?I use project in STM32F3-Discovery_FW_V1.1.0->Peripheral_Examples->USB_Example compile and Download?The PC can regnize HID Device Joy_Stick?but the project in STM32Cube_FW_F3_V1.6.0->STM32F303RE-Nucleo->HID_Standalone demo(STM32Cube\Repository\STM32Cube_FW_F3_V1.6.0\Projects\STM32F303RE-Nucleo\Applications\USB_Device\HID_Standalone) compile and download ,the PC can not regnize the usb device and shows unknow device?HSE 8M?HCLK 72M?and PA11?PA12. The project produced by CubeMX,configed as usb hid is also unknown device?cubemx 4.16.1?lib STM32Cube_FW_F3?How can USB device for STM32F3 be regnized by PC after configed by CUBEMX?
#stm32f3-usb-cubemx2016-10-08 9:33 PM
debug info for pprintf with uart
HAL_PCD_EP_Open,ep_addr=0 HAL_PCD_EP_Open,ep_addr=128 HAL_PCD_SetAddress, address=0 PCD_ReadPMA wNBytes:0PCD_EP_ISR_Handler,(wEPVal & USB_EP_SETUP) != 0,ep->xfer_count=0 HAL_PCD_SetupStageCallback,USBD_LL_SetupStage pdev->request.bmRequest:0 USBD_StdDevReq,req->bmRequest=0 USBD_StdDevReq,req->bRequest=0 USBD_GetStatus,pdev->dev_state=1 USBD_CtlError HAL_PCD_EP_SetStall,ep_addr=128 HAL_PCD_EP_SetStall,ep_addr=0We’re moving the ST Community to a new platform to give you a better and more reliable community experience.