2016-08-13 5:53 PM
Hi Everyone,
I'm trying to do a simple read or write into a usb pendrive (TOSHIBA 4Gb ) using a custom board with a STM32F207VGT6 mcu on it...I developed the firmware with STMCubeMX, by using USB_OTG_FS as HOST_ONLY, with Mass Storage Host Class and FATFs...Here's a part of the code that I used.../* Includes ------------------------------------------------------------------*/
&sharpinclude ''stm32f2xx_hal.h''&sharpinclude ''fatfs.h''&sharpinclude ''rtc.h''&sharpinclude ''tim.h''&sharpinclude ''usart.h''&sharpinclude ''usb_host.h''&sharpinclude ''gpio.h''&sharpinclude ''ff_gen_drv.h''&sharpinclude ''usbh_diskio.h''/* USER CODE BEGIN Includes *//* USER CODE END Includes *//* Private variables ---------------------------------------------------------*//* USER CODE BEGIN PV *//* Private variables ---------------------------------------------------------*//* USER CODE END PV *//* Private function prototypes -----------------------------------------------*/void SystemClock_Config(void);void Error_Handler(void);void MX_USB_HOST_Process(void);/* USER CODE BEGIN PFP *//* Private function prototypes -----------------------------------------------*//* USER CODE END PFP *//* USER CODE BEGIN 0 *//* USER CODE END 0 */ FIL USB_Fil; FATFS USB_Fs; int main(void){ /* USER CODE BEGIN 1 */ /* USER CODE END 1 */ /* MCU Configuration----------------------------------------------------------*/ /* Reset of all peripherals, Initializes the Flash interface and the Systick. */ HAL_Init(); /* Configure the system clock */ SystemClock_Config(); /* Initialize all configured peripherals */ MX_GPIO_Init(); MX_RTC_Init(); MX_TIM4_Init(); MX_USART2_UART_Init(); MX_USART3_UART_Init(); MX_FATFS_Init(); MX_USB_HOST_Init(); uint8_t usb_write =1; uint32_t wbytes; /* File write counts */ uint8_t wtext[] = ''text to write logical disk''; /* File write buffer */ /* USER CODE BEGIN 2 */ /* USER CODE END 2 */ /* Infinite loop */ /* USER CODE BEGIN WHILE */ while (1) { // USER CODE END WHILE MX_USB_HOST_Process(); if((FATFS_LinkDriver(&USBH_Driver,USBH_Path))&&usb_write) { if(f_mount(&USB_Fs, USBH_Path,0) == FR_OK) { if(f_open(&USB_Fil, ''0:/STM32.txt'', FA_CREATE_ALWAYS | FA_WRITE ) == FR_OK) { GPIOD->BSRR = GPIO_PIN_13; usb_write=0; //write once if(f_write(&USB_Fil,wtext, sizeof(wtext), (void *)&wbytes) == FR_OK) { f_close(&USB_Fil); } } } } FATFS_UnLinkDriver(USBH_Path); } /* USER CODE END 3 */}Everytime the result of ''f_open'' funcion is FR_NOT_READY... Why? What I missed? I followed the ''STM32Cube USB host library'' but the result when i called ''f_open'' was the same...Thanks to everyone who spend some time for my real big mistake. #stm32cubemx #stm32f2 #usb #host2016-08-15 7:08 AM
Hi forestan.massimo,
Try to do like the following implementation example:
''char SDPath[4];
f_mount(&SDFatFs, (TCHAR const*)SDPath, 0)
''I recommend that you take a look to the ''FatFs_uSD'' example in STM32CubeF2 package at this path: STM32Cube_FW_F2_V1.3.0\Projects\STM322xG_EVAL\Applications\FatFs\FatFs_uSD
-Hannibal-
2017-01-09 8:42 AM
I have the same problem. I try using ]
f_mount(&SDFatFs, (TCHAR const*)SDPath, 0)
but it's not work
2019-02-25 2:26 AM
Same problem here using STM32F746-Disco
Giampaolo
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.