2021-02-27 11:34 PM
After spending a year or so on different processors, I returned to a new project using the STM32L476 which I had used STM32CubeMX V5.x on before.
Using STM32CubeMX V6.1.1 with MDK 5.27 even the simplest USB CDC serial port device would not work; the windows driver gets part way through initiating the device as a serial port and then fails to open with error code 10. The same settings using CubeMX V5.x did not have this problem.
Other notes:
Using STM32CubeMX V6.1.1 with MDK 5.27 with the same usb cdc configuration but on a STM32L152RC runs perfectly.
With STM32CubeMX V6.1.1 one can ONLY select firmware package STM32Cube FW_L4 V1.16.0, and editing the .ioc file to force an earlier package e.g. STM32Cube FW_L4 V1.13.0 fails to produce compile-able code.
The only GOOD thing is that finally there is a "CDC_TransmitCplt_FS" hook added which I always had to add manually before.
If anyone knows a work around please let me know, otherwise I will have to set up another machine (yet again) for running STM32CubeMX V5.x on.
Thanks.
Solved! Go to Solution.
2021-02-28 12:25 AM
Just found out about the STM32CubeMX 6.2.0 release fixed @ STM32Cube FW_L4 V1.17.0
Installed it and it now works
Aaaargh!!
2021-02-28 12:25 AM
Just found out about the STM32CubeMX 6.2.0 release fixed @ STM32Cube FW_L4 V1.17.0
Installed it and it now works
Aaaargh!!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.