2014-07-30 1:30 AM
Hi,
In the last few days I have spend few hours trying to setup FreeRTOS + LwIP TCP/IP stack. Now it is finally working (UDP echo, ICMP ping), but I believe there might be some bugs in STM32CubeMX. - Interrupt priority for ETH_IRQn is left at default priority which is too low. This causes FreeRTOS hanging at assert. (see ). - Some (important) settings for STM32CubeMX for LwIP don't get transferred into lwiopts.h. This means that default values (which are often 0) are used. I did manually set: &sharpdefine TCPIP_THREAD_STACKSIZE 1000 &sharpdefine TCPIP_MBOX_SIZE 5 &sharpdefine DEFAULT_UDP_RECVMBOX_SIZE 2000 &sharpdefine DEFAULT_TCP_RECVMBOX_SIZE 2000 &sharpdefine DEFAULT_ACCEPTMBOX_SIZE 2000 &sharpdefine DEFAULT_THREAD_STACKSIZE 500 &sharpdefine TCPIP_THREAD_PRIO (configMAX_PRIORITIES - 2) in addition CHECKSUM_BY_HARDWARE didn't get transferred into lwiopts.h so checksums were invalid. The solution was to add the following defines to lwiops.h. &sharpdefine CHECKSUM_GEN_IP 0 &sharpdefine CHECKSUM_GEN_UDP 0 &sharpdefine CHECKSUM_GEN_TCP 0 &sharpdefine CHECKSUM_CHECK_IP 0 &sharpdefine CHECKSUM_CHECK_UDP 0 &sharpdefine CHECKSUM_CHECK_TCP 0 &sharpdefine CHECKSUM_GEN_ICMP 0 With this configuration I have tested UDP echo, pinging and ARP protocol and for now they work. However, I would be nice if authors of STM32CubeMX could check this issue and make sure all set parameters get converted into source code. Thanks, Crt #stm32cubemx-ethernet2014-08-18 2:12 AM
Hello,
Thanks for this contructive feedback. Regarding the ETH_IRQn default priority setting, we are investigating to change this asap. Regarding the manual settings you mentionned for LwIP: - TCPIP_THREAD_STACKSIZE, TCPIP_MBOX_SIZE, DEFAULT_UDP_RECVMBOX_SIZE, DEFAULT_TCP_RECVMBOX_SIZE and DEFAULT_ACCEPTMBOX_SIZE can be set through the LwIP Configuration GUI in ''All LwIP Options / Thread Options'' with the values you manually set so that they will appear correctly set in lwipopts.h - TCPIP_THREAD_PRIO can be set also through the LwIP Configuration GUI in ''All LwIP Options / Thread Options'' but not using a variable like configMAX_PRIORITIES. The right way to do it using a variable like configMAX_PRIORITIES is to set it manually in lwipopts.h in a USER CODE section so that this will be kept at each code generation - CHECKSUM_GEN_IP, CHECKSUM_GEN_UDP, CHECKSUM_GEN_TCP, CHECKSUM_CHECK_IP, CHECKSUM_CHECK_UDP, CHECKSUM_CHECK_TCP, CHECKSUM_GEN_ICMP are also configurable through the LwIP Configuration GUI in ''All LwIP Options / ChecksumOptions'', so that you can set it to Disabled and this will be set automatically in the lwipopts.h after a code generation. You're right, for the moment, automatic setting of all CHECKSUM parameters could be a bit improved, this improvement will be considered. I hope this answer to your feedback. Best Regards, /Eric2014-11-03 2:18 AM
Dear user,
The default value issue you raised has now been solved in the latest STM32CubeMX 4.4 release. Best Regards2015-07-25 5:48 AM
May I know how to set it ? I'm using STM32F107 and DP83848
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.