2020-01-10 2:51 PM
Hi !
After updating I'm not able to load any project or generating a new one.
Each time a project is loaded the program crashes with
...
2020-01-10 23:34:35,765 [INFO] BlockDiagram:1818 - stop enableDisableButtons
java.lang.NullPointerException
...
at java.desktop/java.awt.EventDispatchThread.run(EventDispatchThread.java:90)
Exception in thread "AWT-EventQueue-0" java.lang.NoSuchMethodError: 'boolean com.st.microxplorer.mcu.IP.isDMASupported()'
...Please see attached text file for full log.
2020-01-10 8:58 PM
problem is because of jave
please update java first then try
2020-01-11 12:40 AM
Thanks for your feedback.
But neither a update of java11 nor installing java13 solves the problem. I've attached the full log of both java versions.
> java --version
openjdk 13 2019-09-17
OpenJDK Runtime Environment (build 13+33)
OpenJDK 64-Bit Server VM (build 13+33, mixed mode, sharing)> java --version
openjdk 11 2018-09-25
OpenJDK Runtime Environment 18.9 (build 11+28)
OpenJDK 64-Bit Server VM 18.9 (build 11+28, mixed mode)> lsb_release --all
No LSB modules are available.
Distributor ID: LinuxMint
Description: Linux Mint 19.3 Tricia
Release: 19.3
Codename: tricia
2020-01-11 12:41 AM
2020-01-11 3:17 AM
you should study link related to update
https://community.st.com/s/question/0D50X0000BwjtUBSQY/stm32cubemx-550-released
2020-01-11 6:51 AM
you mean this comment, right ?
STM32CubeIDE toolchain:
• It is functional only with a Java 8 64-bit Java Virtual Machine.
I've used this java version in the past (and STM32CubeMX version 5.4.0 was running fine with that):
> java -version
openjdk version "1.8.0_232"
OpenJDK Runtime Environment (build 1.8.0_232-8u232-b09-0ubuntu1~18.04.1-b09)
OpenJDK 64-Bit Server VM (build 25.232-b09, mixed mode)Although the revision number (?) is 232 I've downloaded the latest available package form java.com which has a revision number of 231
> java -version
java version "1.8.0_231"
Java(TM) SE Runtime Environment (build 1.8.0_231-b11)
Java HotSpot(TM) 64-Bit Server VM (build 25.231-b11, mixed mode)Unfortunately no improvement ...
And the jdk version is not downloadable without an Oracle account.
So currently all installed versions didn't work:
> sudo update-alternatives --config java
There are 4 choices for the alternative java (providing /usr/bin/java).
Selection Path Priority Status
------------------------------------------------------------
0 /usr/lib/jvm/java-8-openjdk-amd64/jre/bin/java 1081 auto mode
1 /usr/lib/jvm/java-8-openjdk-amd64/jre/bin/java 1081 manual mode
2 /usr/lib/jvm/jdk-11/bin/java 0 manual mode
3 /usr/lib/jvm/jdk-13/bin/java 0 manual mode
* 4 /usr/lib/jvm/jre1.8.0_231/bin/java 0 manual mode
Press <enter> to keep the current choice[*], or type selection number:
2020-01-13 11:12 AM
Finally a fresh install of STM32CubeMx solved the problem !
2020-02-04 4:46 AM
Hi Michael
What java version are you finally using?
2020-02-04 9:07 AM
Hi Christian,
obviously the "only Java 8" statement is not true ;)
I'm running jdk-13
> java -version
openjdk version "13" 2019-09-17
OpenJDK Runtime Environment (build 13+33)
OpenJDK 64-Bit Server VM (build 13+33, mixed mode, sharing)
2020-02-04 1:18 PM
Thanks for you answer
I have java 8 now and after a clean install of CubeMX 5.5.0, it actually works fine now
$ java -version
openjdk version "1.8.0_242"
OpenJDK Runtime Environment (build 1.8.0_242-8u242-b08-0ubuntu3~18.04-b08)
OpenJDK 64-Bit Server VM (build 25.242-b08, mixed mode)(I had java 11 before and CubeMX 5.4.0 was working fine with it)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.