2018-01-18 12:18 AM
Hello,
I've encountered a bug in code generation when using the LL STM32F3 drivers 1.9.0 in Cube 4.23.0.
The device is the
STM32F303CCTx
, although it's probably not device specific.Using the clock configurator and setting an HSE of 16MHz, the code generated in
stm32f3xx_ll_rcc.h
indicates a wrong value for HSE:
&sharpif !defined (HSE_VALUE)
&sharpdefine HSE_VALUE 8000000U /*!< Value of the HSE oscillator in Hz */&sharpendif /* HSE_VALUE */This can cause all sorts of problems if one uses the API to get various peripheral clock speeds, like
LL_RCC_GetUSARTClockFreq
which gave me the wrong value, causing me to set up the wrong baud.The
.ioc
file seems correct since the relevant field is correct:RCC.HSE_VALUE=16000000
#ll-drivers #stm32f3 #cube-mx2018-05-07 12:55 AM
Yes, project-wide definition solves that problem, but my primary point was that Cube software in similar conditions of sole LL usage genarates inoperable code with not so easy to find bu
g but that is already known for a couple of months. While this problem is not fixed even with such a simple solution I think many developers using Cube for LL will have to make the same debugging way as I did.
2018-05-10 2:47 PM
I haven't verified on a board but isn't the real problem the order of the includes in main.c?
swap the order the includes:
#include 'stm32l0xx_hal.h'
#include 'main.h'This compiles and should give the right answer since
stm32l0xx_hal.h includes
stm32f3xx_hal_conf.h which will now be included before stm32f1xx_ll_rcc.h.
This would be a fix to the STM32CubeMX code generator.
2018-05-11 4:09 AM
As I have mentioned above that won't help much because HSE frequency definition in this case will only take effect for main.c file compilation. Since there are still lots of LL's .c files and each one of these requires its own compilation process with its own separate defines (obviously not including any half_conf.h at all), every such .c file will get only default HSE_VALUE of 8000000 that is defined inside LL's headers making library functions see only this value.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.