2019-03-11 5:37 AM
I can't measure tempsensor with vbat and vref because cubemx generates low layer code in the following order:
LL_ADC_REG_SetSequencerRanks(ADC1, LL_ADC_REG_RANK_6, LL_ADC_CHANNEL_TEMPSENSOR);
LL_ADC_SetChannelSamplingTime(ADC1, LL_ADC_CHANNEL_TEMPSENSOR, LL_ADC_SAMPLINGTIME_640CYCLES_5);
LL_ADC_SetChannelSingleDiff(ADC1, LL_ADC_CHANNEL_TEMPSENSOR, LL_ADC_SINGLE_ENDED);
LL_ADC_SetCommonPathInternalCh(__LL_ADC_COMMON_INSTANCE(ADC1), LL_ADC_PATH_INTERNAL_TEMPSENSOR);
/** Configure Regular Channel
*/
LL_ADC_REG_SetSequencerRanks(ADC1, LL_ADC_REG_RANK_7, LL_ADC_CHANNEL_VREFINT);
LL_ADC_SetChannelSamplingTime(ADC1, LL_ADC_CHANNEL_VREFINT, LL_ADC_SAMPLINGTIME_640CYCLES_5);
LL_ADC_SetChannelSingleDiff(ADC1, LL_ADC_CHANNEL_VREFINT, LL_ADC_SINGLE_ENDED);
LL_ADC_SetCommonPathInternalCh(__LL_ADC_COMMON_INSTANCE(ADC1), LL_ADC_PATH_INTERNAL_VREFINT); // Previously enabled tempsensor bit get overwritten here and only internal vrefint channel is enabled.. I took a few hours until I figured out why ny MCU temp measuring module isn't works since I ported my ADC to HAL from LLFinaly result is only vrefint is enabled and tempsensor is disabled. CubeMX should use logical OR in this case. In HAL it is implemented correctly, but this implementation missing from LL.
Solution is:
LL_ADC_SetCommonPathInternalCh(__LL_ADC_COMMON_INSTANCE(ADC1), LL_ADC_PATH_INTERNAL_TEMPSENSOR | LL_ADC_PATH_INTERNAL_VREFINT);
2019-03-20 11:08 PM
Any news please?
2019-04-17 12:26 AM
Any news on this issue?
2019-04-26 12:09 AM
Please look after this bug,. it's still present with CubeMX 5.2.0.
2019-04-26 11:07 AM
Just adding my name to the thread so I can track this.
2019-10-01 1:19 AM
Any news on this please?
2019-10-02 8:26 AM
Hello @kurta999 ,
Could you please share your ioc file?
Best Regards,
Khouloud.
2019-10-03 12:17 AM
2019-10-03 2:34 AM
Thanks for the feedback, this's reported internally for further check.
Best Regards,
Khouloud.
2019-10-03 11:12 PM
Thanks!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.