2019-01-18 1:20 PM
When selecting "Makefile" for Toolchain/IDE with the STM32F4 Family of MCU's, a Linker Script is generated with a license that does not allow the code to be used with anything other than "System Workbench".
** (c)Copyright Ac6.
** You may use this file as-is or modify it according to the needs of your
** project. Distribution of this file (unmodified or modified) is not
** permitted. Ac6 permit registered System Workbench for MCU users the
** rights to distribute the assembled, compiled & linked contents of this
** file as part of an application binary file, provided that it is built
** using the System Workbench for MCU toolchain.
2019-01-18 1:38 PM
I have been using Cube MX for the last month and Keil. Cube MX would generate all the initialization codes for project and open automatically Keil. I have not seen any problems so far.
As far as I know Cube MX is free to download and use.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.