2021-07-21 11:31 PM
What is new in STM32CubeMX V6.3.0
• Added the support for new part numbers in the STM32U5 Series:
STM32U575A(G-I)Ix, STM32U575A(G-I)IxQ, STM32U575C(G-I)Tx,
STM32U575C(G-I)TxQ, STM32U575C(G-I)Ux, STM32U575C(G-I)UxQ,
STM32U575O(G-I)YxQ, STM32U575Q(G-I)Ix, STM32U575Q(G-I)IxQ,
STM32U575R(G-I)Tx, STM32U575R(G-I)TxQ, STM32U575V(G-I)Tx,
STM32U575V(G-I)TxQ, STM32U575Z(G-I)Tx, STM32U575Z(G-I)TxQ,
STM32U585AIIx, STM32U585AIIxQ, STM32U585CITx, STM32U585CITxQ,
STM32U585CIUx, STM32U585CIUxQ, STM32U585OIYxQ, STM32U585QIIx,
STM32U585QEIxQ, STM32U585RITx, STM32U585RITxQ, STM32U585VITx,
STM32U585VITxQ, STM32U585ZITx and STM32U585ZETxQ
• Added the support for 3 new boards related to the STM32U5 Series: B-U585I-IOT02A,
NUCLEO-U575ZI-Q and STM32U575I-EV
• Added the support for 2 new boards related to the STM32MP1 Series:
STM32MP157D-DK1 and STM32MP157D-EV1
• Added the support for 1 new board related to the STM32L4 Series:
STEVAL-STWINKT1B
• Added the support for SMBUS Fast mode plus and SMBUS fast mode for the STM32G0 Series, the STM32WL Series and the STM32WB Series
• Added the support for RAMECC in the STM32H7 Series
• Added the support for PWR secure configuration for the STM32L5 Series in Arm® TrustZone®-activated projects (TZEN=1)
• Added updates for the installation procedure with the JRE™ bundling support. The bundled JRE™ is updated to AdoptOpenJDK-11.0.10+9 and JavaFX-11.0.2
• Added the support for STM32CubeMX updates with the https protocol
• Added license click-through: the user can accept the firmware package license terms
before any download
• Added thread-safe locking support. It can be enabled or disabled in [Project
manager]>[Project] Thread-safe Settings
• Added the support of the cohabitation between Azure® RTOS USBX or USB and USBPD
for the STM32U5 Series and STM32G0 Series, making it possible to enable and disable the USB support from USB-PD middleware
Known limitations
Please refer the the release note
Main fixed issues
Link
2021-10-04 3:14 PM
Attention!
File "Repository\STM32Cube_FW_F4_V1.26.2\Drivers\CMSIS\Core\Include\core_cm4.h"
Line 411 "uint32_t RSERVED1[24U];"
There must be RESERVED1, not RSERVED1.
2022-02-02 1:11 PM
Hello @Alexander CZAJOR @Nawres GHARBI
I cannot get Aure to compile on the 735DK kitI have asked repeatably and no-one at ST is capable of compiling code.
Please check my posts and use a fresh machine and find the bug in your install.
MQTT Azure sample does not work on the fresh install of windows.
I have spent many thousands of hours helping your clients for free, now you need to help me once...
Can anyone at st compile code ?
Nick
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.