2019-06-13 11:20 PM
STM32CubeMX-5.2.1 - why I can't install it in d:\STM32\STM32CubeMX path?
I use d:\STM\ for \STM32 ST-LINK Utility\ , \STMStudio\ and other STM application. Why not CubeMX?
Setup returns error: Invalid directory path. Please enter a directory path meets the operation system's requirements.
2019-07-30 2:23 AM
Same problem to me, on Windows 10 (64 bit), no install directory will make it happy, I cannot install the software.
2019-08-08 4:06 PM
You need to use capitalized drive letter "D" instead of "d"
Then it should work fine.
2019-08-27 1:10 AM
Thanks a lot, it works.
This is a really stupid bug, but your answer is of great use!
2020-08-23 11:56 AM
GokhanBektas thanks for the contribution please but sometimes capitalizing the drive letter doesn't work . When I faced the same problem, I only when into that directory/path and permanently deleted the folder STM32Cube, then when I continued with the installation, it went on successfully.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.