2024-03-27 11:29 PM
I'm using the Nucleo-C031C6 board, and I chose this (NUCLEO-C031C6) from the board selector when starting the IDE. (STM32CubeIDE v1.15).
I tried switching Timebase Source (in SYS menu) from SysTick to TIM16, then when I compiled, I got this error:
../Core/Inc/stm32c0xx_hal_conf.h:237:11: fatal error: stm32c0xx_hal_tim.h: No such file or directory
It is just a bare project with no user code added.
I had to switch from SysTick to TIM16 because I was trying out ThreadX.
Solved! Go to Solution.
2024-03-28 12:26 AM - edited 2024-03-28 2:25 AM
Hello @JLoh
You have to check your Paths and include the path of this HAL Driver.
For this issue, I've been able to reproduce it and I will escalate it internally for correction (in internal ticket number 177285).
Thank you for reporting This.
Best Regards
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-03-27 11:49 PM
It seemed to me that the necessary files weren't copied. To workaround this, I just enabled another Timer (TIM16) and this bug disappeared.
2024-03-28 12:26 AM - edited 2024-03-28 2:25 AM
Hello @JLoh
You have to check your Paths and include the path of this HAL Driver.
For this issue, I've been able to reproduce it and I will escalate it internally for correction (in internal ticket number 177285).
Thank you for reporting This.
Best Regards
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-04-20 5:59 PM
Hello.
Do you have any news about internal ticket 177285 to this bug?
I want to try Threadx with this MCU.
Thank you very much.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.