2018-02-02 10:15 AM
Hello, I will first describe what I am trying to accomplish, what I have tried, and how it is not working; any help/advice is greatly appreciated.
I have an external MCU (Particle Photon) acting as the SPI Master. Approximately every half second it needs to send 64 bytes to the STM32F103. It can also be multiples of 64 bytes (e.g. 50x 64 byte chunks equaling 3,200 bytes in this example... maximum of 200x chunks). The STM32 also has its own data that needs to be sent back to the master MCU, same format.
I have stripped a lot of this down, and am just trying to get a single 64 byte exchange to happen reliably, and I am failing at that.
I used STM32CubeMX to generate the source code and configurations. Here are the functions I am using:
SPI Buffers & Init Flag:
uint8_t txData[64]; //uint8_t txData[MAX_DEVICES_TRACKED * 64];
uint8_t rxData[64]; //uint8_t rxData[MAX_DEVICES_TRACKED * 64]; bool spiReady = true;Main Loop:
while(true)
{ if(spiReady) { spiReady = false; InitSPISlave(&hspi1); } }Init SPI:
void InitSPISlave( SPI_HandleTypeDef *spiHandler )
{ memset(rxData, 0, sizeof(rxData)); HAL_SPI_TransmitReceive_IT(spiHandler, txData, rxData, sizeof(txData));}Callbacks That Occur After SPI TXRX Complete, And Error Callback:
void HAL_SPI_TxRxCpltCallback(SPI_HandleTypeDef *hspi)
{ printf('SP1 Data Received: '); for(int i = 0; i < 64; i++) { printf('%lx ', (long)rxData[i]); } printf('\n');memset(txData, 0, sizeof(txData)); //If I don't clear the data, it comes across ok
spiReady = true;
}
void HAL_SPI_ErrorCallback(SPI_HandleTypeDef *hspi)
{ printf('SPI1 ERROR: %d \n', hspi->ErrorCode); spiReady = true; }For testing purposes I have a timer that periodically populates the txData buffer. As soon as the transaction is complete, and the master MCU has the data, I want to clear out the txData buffer.... when more data becomes available it will then go into the txData, which is what the timer is simulating.
I am experiencing 2 problems:I tried switching over to DMA SPI, e.g. 'HAL_SPI_TransmitReceive_DMA(spiHandler, txData, rxData, sizeof(txData));', and while it is slightly quicker to initialize-still way too slow, I experience the same problems.
I have been scouring the internet trying to read up on this, and most people say the HAL drivers don't work right, and to work directly with the registers yourself. If this is the case, I don't know where to start in accomplishing that... or if maybe there is a fix I can do to get this up and running?
Any help on working through this is greatly appreciated, thanks!
#stm32 #spi #slave #stm32cubemx #hal2018-02-02 2:56 PM
printf in embedded is a bad idea, and in ISR is a disaster.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.