2025-06-09 9:57 AM - last edited on 2025-06-09 9:59 AM by Andrew Neil
hi there
could you help me with this;
after updating CUBMX to latest one 6.14.1, does not open the project automatically , even when i open it from IDE with existing project from CUB MX option , still comes up with this error ;
This file has been generated with STM32CubeMX version '6.14.1'.Your current STM32CubeMX version is '6.4.0'.
Please check for update: Help > Check for Updates
THE FUNNY THING IS THE LATEST UPDATE FOR CUB MX IS 6.14.1 SO WHY DETECTS THE VERSION WRONG, WHICH IS NOT EXIST ( 6.4)!?
SO I CAN NO LUNCH PROJECT FROM CUB MX TO IDE either.
could you help me with this?
regards
Ali10
2025-06-09 10:18 AM - edited 2025-06-09 10:19 AM
STM32CubeIDE has a bundled STM32CubeMX version. When you open an IOC from within STM32CubeIDE, it uses this bundled version. The only way to update the bundled STM32CubeMX it is to update STM32CubeIDE itself. You can either do that or you can leave it as-is and use the standalone STM32CubeMX to open it. Either way works.
2025-06-09 10:59 AM
@Ali10 Well... from STM32CubeIDE 2.0 everything will be better and hopefully clearer.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.