2025-02-06 11:32 AM
I have created a project for the STM32H747I-DISCO and have deadlocked the MCU twice. a BIG thanks to ST for not having ANY warning about this.
The DISCO board comes configured to default to SMPS mode. The project I created, without any warnings, defaulted to LDO mode. I corrected the problem using the process described in UM2411, section 5.2.3 only to go right back into the deadlock condition when downloading code.
I now know that I must set the power mode to SMPS but I cannot find this setting in CubeMX.
I am using CubeIDE v1.17.0. Where is the power settings for LDO and SMPS?????
Solved! Go to Solution.
2025-02-13 9:45 AM - edited 2025-02-13 9:46 AM
I modified my STM32H747I-DISCO by first placing a slide switch across R192 and also to convert it to LDO instead of SMPS. UM2411, Section 5.2.3
• LDO mode:
– SB1, SB12, SB49 mounted
– SB2, SB11, SB19, SB46, SB48 removed
I then configured my debugs as shown in the below ST video (at near time 10:30)
https://www.youtube.com/watch?v=k3mXhPZSasw
The video instructs to check the box "Halt all cores". Things didn't work until I UNCHECKED the box "Halt all cores". I now have a working, debuggable STM32H747I-DISCO with an H747 that runs at 480MHz which is what I wanted.
Thank you all!
2025-02-06 12:28 PM
https://community.st.com/t5/stm32cubemx-mcus/stm32h725-smps-issue/td-p/763986
2025-02-06 12:43 PM
Most probably it's an issue pointed out by @Tesla DeLorean
There is a limitation in CubeMx 6.13.CubeIDE v1.17.0. It will be fixed as soon as possible.
2025-02-06 1:01 PM
>>I have created a project for the STM32H747I-DISCO and have deadlocked the MCU twice. a BIG thanks to ST for not having ANY warning about this.
I think I immediately bricked my H747I-DISCO about 7 years ago, and after doing the BOOT0 R192, had suggested a BOOT0 switch somewhere accessible, way back then. Same issue with the H745 / H750 DISCO's. I recollect there being an STM32 Cube Programmer "Access Port" trick too, but I don't recollect how that worked. These days I solder a right-angle jumper on the NUCLEO-144 H7 boards between VDD and BT0
2025-02-13 9:45 AM - edited 2025-02-13 9:46 AM
I modified my STM32H747I-DISCO by first placing a slide switch across R192 and also to convert it to LDO instead of SMPS. UM2411, Section 5.2.3
• LDO mode:
– SB1, SB12, SB49 mounted
– SB2, SB11, SB19, SB46, SB48 removed
I then configured my debugs as shown in the below ST video (at near time 10:30)
https://www.youtube.com/watch?v=k3mXhPZSasw
The video instructs to check the box "Halt all cores". Things didn't work until I UNCHECKED the box "Halt all cores". I now have a working, debuggable STM32H747I-DISCO with an H747 that runs at 480MHz which is what I wanted.
Thank you all!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.