2020-09-04 3:17 AM
In CubeIDE 1.4 in the graphical configurator, using a STM32F091, if you select the PA8 pin function as MCO,
the generated code in main.c / GPIO init will configure the pin as AF0 with LOW speed.
This should really be HIGH speed, it doesn't get any higher than the system clock frequency ;) And you won't see much on the scope with that limited analog bandwidth, when you configure this for the purpose of checking whether the MCU really runs at the desired clock speed.
Solved! Go to Solution.
2020-09-04 4:05 AM
Hello @Community member
You can change the Speed using MX under GPIO .
Thanks
Khouloud
2020-09-04 4:05 AM
Hello @Community member
You can change the Speed using MX under GPIO .
Thanks
Khouloud
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.