2019-01-24 12:14 AM
Hi. I need to create USB MSC Device on STM32F407. I use CubeMX for create project. When I compiled the project with MSC_MEDIA_PACKET = 512 windows did not see the mass storage device, then I changed MSC_MEDIA_PACKET = 256 and windows saw the mass storage device and also offered to format it. I also did projects on stm32f0 and stm32f3 with MSC_MEDIA_PACKET = 512, everything worked without problems for them, Windows found the device and offered to format the disk. How to do when define MSC_MEDIA_PACKET = 512 for Windows to see it?
Solved! Go to Solution.
2019-01-28 2:27 AM
I increased the minimum heap size and minimum stack size in advanced settings and this fixed the problem
2019-01-28 2:27 AM
I increased the minimum heap size and minimum stack size in advanced settings and this fixed the problem
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.