cancel
Showing results for 
Search instead for 
Did you mean: 

NUCLEO-L073RZ + SX1272MB2DAS LoRa and I-CUBE-LRWAN

jaimadafaca
Associate II

Hello all,

I have a NUCLEO-L073RZ with SX1272MB2DAS LoRa RF Expansion board and I’m not being able to run the firmware “End_Node�? provided in I-CUBE-LRWAN (1.2.0).

The problem comes when “SystemClock_Config�? is called in main:

void SystemClock_Config( void )

{

 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 RCC_OscInitTypeDef RCC_OscInitStruct = {0};

 /* Enable HSE Oscillator and Activate PLL with HSE as source */

 RCC_OscInitStruct.OscillatorType     = RCC_OSCILLATORTYPE_HSI;

 RCC_OscInitStruct.HSEState           = RCC_HSE_OFF;

 RCC_OscInitStruct.HSIState           = RCC_HSI_ON;

 RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;

 RCC_OscInitStruct.PLL.PLLState       = RCC_PLL_ON;

 RCC_OscInitStruct.PLL.PLLSource      = RCC_PLLSOURCE_HSI;

 RCC_OscInitStruct.PLL.PLLMUL         = RCC_PLLMUL_6;

 RCC_OscInitStruct.PLL.PLLDIV         = RCC_PLLDIV_3;

 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)

 {

   Error_Handler();

 }

The HAL_RCC_OscConfig(&RCC_OscInitStruct) function always return a HAL_ERROR and the goes to Error_Handler();

I’ve checked inside HAL_RCC_OscConfig function, and it seem that something wrong with PLL configuration in the next instruction:

   if(__HAL_RCC_GET_SYSCLK_SOURCE() != RCC_SYSCLKSOURCE_STATUS_PLLCLK)

Does anybody know why is not well initialized the clock in this Nucleo board?

Really I don’t understand, because it in and example downloaded from ST and also using an original bord

Sure I’m doing something wrong but I don’t see what.

I’m using IAR Worknbench 8.10.1

Thank you for your help,

Best regards,

Jai

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
jaimadafaca
Associate II

I'm still with the same problem :(

Could anybody help me please?

Thank you for your help,

Regards,

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.