2020-12-12 1:21 AM
Hello,
Updated STM32CubeMX Version 6.1.0.
After an update, I opened my previous version .ioc file (CONTROLLER:STM32G070RB) and only changing baud-rate in UART parameter setting, generated MDK-ARM V_2.7 KEIL uVision file. I opened that generated file and compiled it.
BUT IT SHOWS 5 ERRORS WHICH I MENTIONED BELOW, WERE NOT CONCERNED TO THE CHANGES I MADE IN CUBE UART BAUD-RATE PARAMETER.
These errors are troubling me, please help me out from this bug !!!
ERROR MESSAGES:
*** Using Compiler 'V5.06 update 7 (build 960)', folder: 'C:\Keil_v5\ARM\ARMCC\Bin' Build target 'TemeratureRelay_V1' compiling system_stm32g0xx.c...
../Src/system_stm32g0xx.c(231): error: #20: identifier "RCC_CFGR_SWS_HSE" is undefined case RCC_CFGR_SWS_HSE: /* HSE used as system clock */
../Src/system_stm32g0xx.c(235): error: #20: identifier "RCC_CFGR_SWS_LSI" is undefined
case RCC_CFGR_SWS_LSI: /* LSI used as system clock */
../Src/system_stm32g0xx.c(239): error: #20: identifier "RCC_CFGR_SWS_LSE" is undefined
case RCC_CFGR_SWS_LSE: /* LSE used as system clock */
../Src/system_stm32g0xx.c(243): error: #20: identifier "RCC_CFGR_SWS_PLL" is undefined case RCC_CFGR_SWS_PLL: /* PLL used as system clock */
../Src/system_stm32g0xx.c(264): error: #20: identifier "RCC_CFGR_SWS_HSI" is undefined
case RCC_CFGR_SWS_HSI: /* HSI used as system clock */
../Src/system_stm32g0xx.c: 0 warnings, 5 errors
Target not created.
Thanks & regards
Contact Mail Id: ZAINULAABEDIN.S@GMAIL.COM
2020-12-12 1:28 AM
Only tips, when you have old backup compare , or try delete file system_stm32g0xx... from folder. MX generates starting in main maybe.
2020-12-12 2:50 AM
thanks for your response.
but for time being I attempted to comment the whole function " void SystemCoreClockUpdate(void) " which was generating UNDEFINED IDENTIFIER ERROR. And as a result all error skipped by compiler.
The thing remains is that: I want to know, Whether I had done is OK or not? and Whether that function is having actual significance in my code or not?
2020-12-12 2:50 AM
thanks for your response.
but for time being I attempted to comment the whole function " void SystemCoreClockUpdate(void) " which was generating UNDEFINED IDENTIFIER ERROR. And as a result all error skipped by compiler.
The thing remains is that: I want to know, Whether I had done is OK or not? and Whether that function is having actual significance in my code or not?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.