2020-12-10 12:04 AM
using Nuleo-401RE EVAL and x-cube-spn3-Stepper Motor sample project for expansion board. want to use UART2 and change FLAG pin to PA0. In STM32 Cube IDE I am not able edit back the pin configuration (.ioc not visible in sample project), how to change or re-assign the pins and re-generate code, need to go back Cube Mx? or can we do with Cube IDE we can modify pin assignement?
Solved! Go to Solution.
2020-12-10 11:56 PM
Unfortunatelly no way. If example is delivered without any .ioc file. You have to reverse engineering here, starting a brand new project being able to benefit of device configuration tool.
2020-12-10 12:08 AM
Hello @TVeng.1
It will be more easily if you configure your pins through CubeMX then re-generate code.
Thanks, Khouloud
2020-12-10 1:22 AM
Thanks, I thought same but I want to re-use expansion board powerstepper1 driver and example application.
If I re-generate how to include this example application and driver again on top of newly generated BSP?
2020-12-10 8:46 PM
X-CUBE-SPN3 (High power stepper motor driver software expansion for STM32Cube) is the example project I am trying to modify, I am not seeing .ioc file in that to modify the pin and rebuild source code. Anyway to get the .ioc file? please help.
2020-12-10 11:56 PM
Unfortunatelly no way. If example is delivered without any .ioc file. You have to reverse engineering here, starting a brand new project being able to benefit of device configuration tool.
2020-12-11 1:21 AM
Thank you for clarifying
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.