2021-10-27 2:04 AM
Hi All,
I am working on my Nucleo-L4R5ZI board and facing issues with firmware sdk packages downloaded by "Stm32cubeMx" and "Stm32CubeIDE" software respectively.
I am just trying to test the board using simple led toggle program but it unable to make it toggle properly and tested in other different IDE but issues remain same & present.
Then I have tested it some older developed program using keil IDE it works in that environment, means in older firmware packages it works but not in new latest ones.
(Note - My older firmware packages was deleted and after setting up new Stm32CubeMx it downloads new latest which is not working with my board)
I request you all to please share the possible solution for the same.
I am sharing my very simple and basic IOC file to re-create & perform the same for testing.
Thanks & Regards
SS
2021-10-27 7:05 AM
Debug the code and see where it gets stuck.
You can download older firmware packages in Help -> Manage Embedded Software Packages...
2021-10-30 1:31 PM
it get stuck in the "HAL_Delay(1000)" statement and never comes out of it. As I always start with basic gpio toggle program to check my board but with newer software packages it is not working properly.
I request you please use my above shared .ioc file configuration for the stm32l4r5zi board and try to toggle PC7 pin at 1 sec you come to know exactly what is the issue.
Please suggest the solution for the same.
2021-10-30 1:47 PM
HAL_Delay blocking suggests SysTick is not getting handled correctly. Perhaps the vector table is not initialized correctly, or perhaps interrupts are disabled, or perhaps you're calling it within an interrupt with higher priority.
Ensure SCB->VTOR is being set correctly at startup to the start of your vector table, typically 0x08000000.
An IOC file doesn't contain user code, so sharing that alone doesn't show us what you're doing.
2021-10-31 1:31 AM
Hi TDK,
I am not making any configuration additional, just making one GPIO - PC7 output only for making Led toggle on Eval kit before starting project.
And not touching any thing extra at initial stage, like any interrupt setting & all.
Even I never used to change any of the vector table address in any of my projects, everything is as it is at default conditions.
And I am sharing my project for reference with the all the file, Please let me know the error or modification required.
Looking forward for your responses ...
Thanks & Regards
SS
2021-10-31 7:22 AM
Not sure what to make of this:
// below is changes found form the keil ide led blink demo
/*
* Configure the Systick interrupt time
*/
HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq()/1000);
/*
* Configure the Systick
*/
HAL_SYSTICK_CLKSourceConfig(SYSTICK_CLKSOURCE_HCLK);
/* SysTick_IRQn interrupt configuration */
HAL_NVIC_SetPriority(SysTick_IRQn, 0, 0);
// here it ends for the led blink demo fileThe comments don't look like generated code. Are these lines also in the CubeIDE project you're running or just in Keil?
2021-10-31 1:57 PM
Hi,
Please ignore above statement from the shared example code, I was just testing the above statements from the running the keil project.
It was just for testing purpose you remove this section and comparing the two different projects to identify the changes.
I was comparing the simple generated the stm32cubemx code generator firmware file to figure out the solutions.
It will be great if you can share your feedback for the running the simple Led toggle, as I mentioned about facing issue after new firmware packages installation.
I have tested all the test point you mentioned above regarding the vector table addresses all the setting are kept unchanged/untouched.
Please share us solution for the same.
2021-11-04 1:48 AM
Hi
awaiting for your response !!!
Please share possible solution for the same.
Regards
SS
2021-11-04 2:38 AM
I have compiled your project as is under CubeIDE => works.
Generated EWARM from your .ioc => works.
Check the board for something wrong.
2021-11-04 3:48 AM
Hi,
Can you please share me your code so that I can check the same.
And it will be great if you can share me some check points to verify the board is properly working or not.
(my board is STM32 Nucleo L45ZI)
Regards
SS
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.