2017-12-06 10:03 AM
In CubeMX (ver: 4.23 mcu: STM32F427) I'm trying to define two ports PE10 and PB10 as GPIO_EXTI10 (I need to get edge interrupt on either one).
However, in the 'Pinout' view, when I click GPIO_EXTI10 for PB10 and then for PE10, PB10 is erased (the green turn white). Am I trying to do something that is not possible at all or is it only a limitation of CubeMX?Is there another way to do it in CubeMX?
#cubemx #stm32f4 #exti2017-12-06 10:12 AM
There's no way to do it on the chip, that's why there's no way to do it in CubeMX.
Read the External interrupt/event line mapping subchapter of Interrupts chapter of RM0090.
JW
2017-12-06 11:14 AM
Only one pin at each index, so can't have multiple Pin#10
Want PB10, PA11, PA12, etc
2017-12-06 11:16 AM
That was quick... thank you for the reference, I'll read that.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.