2020-06-15 5:45 AM
As far as I read datasheet it says there is a support for that, but in STM32CubeIDE under FMC I cannot select NAND. There is simply no option for that. See attached file.
Solved! Go to Solution.
2020-09-03 2:57 PM
2020-06-15 7:03 AM
Click NE1 Chis select and you can continue
2020-06-15 10:02 AM
Actually if I check the NE1 there is no NAND option. Only NOR, RAM or LCD....
So, no I cannot continue...
2020-06-15 12:03 PM
It appears that there is only one NAND chipselect, NCE3, and that is not present on the 100-pin package. The footnote to Tab.2 in DS10693 Rev 7, mentioning NCE2, is probably copy-paste from the 'F40x datasheet.
@Imen DAHMEN , can you please have a look at this issue? Does the 'F446 have FMC_NCE2 or not?
Thanks,
JW
2020-06-17 10:13 AM
I raised this internally for check and will come back to you with update.
2020-06-17 11:41 AM
Thanks, Imen.
Jan
2020-09-03 2:57 PM
Fixed in rev.8 of 'F446 DS.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.