2018-11-17 6:54 PM
Hello
It may stop with the interrupt routine of HardFault_Handler.
MCU: STM32F446VCTx
Tools: CubeMX
IDE: IAR Embedded Workbench IDE
This routine is in stm32f4xx_it.c.
void HardFault_Handler(void)
{
/* USER CODE BEGIN HardFault_IRQn 0 */
/* USER CODE END HardFault_IRQn 0 */
while (1)
{
}
/* USER CODE BEGIN HardFault_IRQn 1 */
/* USER CODE END HardFault_IRQn 1 */
}
Currently the status of the following registers is confirmed.
CFSR: Settable Fault Status Register INVSTATE bit is 1.
BFAR: The bus fault address register is 0xE000EDF8.
Registers above seem to be involved.
If you have detailed information, please explain the comment.
Attention, I am Japanese. This content is based on Google translation.
2018-11-17 7:23 PM
Check you have adequate heap and stack to accommodate what you are doing.
Try to identify the instructions that are faulting, a while(1) loop is not very helpful for that.
In Keil I have this
HardFault_Handler\
PROC
EXPORT HardFault_Handler [WEAK]
TST lr, #4 ; Determine correct stack
ITE EQ
MRSEQ R0, MSP ; Read MSP (Main)
MRSNE R0, PSP ; Read PSP (Process)
MOV R1, R4 ; Registers R4-R6, as parameters 2-4 of the function called
MOV R2, R5
MOV R3, R6 ; sourcer32@gmail.com
EXTERN hard_fault_handler_c
B hard_fault_handler_c
ENDPvoid hard_fault_handler_c(unsigned int * hardfault_args, unsigned int r4, unsigned int r5, unsigned int r6)
{
printf ("\n[Hard Fault]\n"); // After Joseph Yiu
printf ("r0 = %08X, r1 = %08X, r2 = %08X, r3 = %08X\n",
hardfault_args[0], hardfault_args[1], hardfault_args[2], hardfault_args[3]);
printf ("r4 = %08X, r5 = %08X, r6 = %08X, sp = %08X\n",
r4, r5, r6, (unsigned int)&hardfault_args[8]);
printf ("r12= %08X, lr = %08X, pc = %08X, psr= %08X\n",
hardfault_args[4], hardfault_args[5], hardfault_args[6], hardfault_args[7]);
printf ("bfar=%08X, cfsr=%08X, hfsr=%08X, dfsr=%08X, afsr=%08X\n",
*((volatile unsigned int *)(0xE000ED38)),
*((volatile unsigned int *)(0xE000ED28)),
*((volatile unsigned int *)(0xE000ED2C)),
*((volatile unsigned int *)(0xE000ED30)),
*((volatile unsigned int *)(0xE000ED3C)) );
while(1);
}
2018-11-17 8:15 PM
Thank you for reply.
I'll give it a try.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.