2021-02-21 10:00 AM
Info : STM32F746NGHx.cpu: hardware has 8 breakpoints, 4 watchpoints
Info : Listening on port 3333 for gdb connections
target halted due to debug-request, current mode: Thread
xPSR: 0x01000000 pc: 0x0800b664 msp: 0x20050000
Info : Stlink adapter speed set to 1800 kHz
adapter speed: 1800 kHz
** Programming Started **
auto erase enabled
Info : flash size probed value 1024
target halted due to breakpoint, current mode: Thread
xPSR: 0x61000000 pc: 0x20000084 msp: 0x20050000
wrote 65536 bytes from file Debug/PeripheralsTrial.elf in 1.273580s (50.252 KiB/s)
** Programming Finished **
** Verify Started **
target halted due to breakpoint, current mode: Thread
xPSR: 0x61000000 pc: 0x2000002e msp: 0x20050000
verified 47680 bytes in 0.160581s (289.963 KiB/s)
** Verified OK **
** Resetting Target **
shutdown command invoked
I see that there are 8 breakpoints and 4 watchpoints in stmWorkbench. But I did not find which part of the project has this. I have also tried selecting option of 'remove all breakpoints in project' But still this error persists. Please help me with this. Im unable to start any project.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.