2021-07-24 2:41 AM
STM32CubeMX Version 6.3.0 "Manage embedded software packages"
When I try to load packages from STMicroelectronic, I always get the error message
"STMicroelectronics.X-CUBE-***.pack (HTTP Access Forbidden)"
The other categories (STM32 Cube MCU Packages or ARM) do not have this problem.
Regards
Rolf
Solved! Go to Solution.
2021-07-26 12:23 AM
The outage should now be resolved, please confirm the resolution on your side too.
2021-07-24 12:37 PM
I am having the exact same problem. I am trying to start a project in STM32CubeIDE 1.6.1 with an STM32F746G-DISCO board and cannot because I cannot download the required firmware package.
2021-07-24 8:27 PM
I don't have an answer ... just the same problem Rob has. Starting a new project from IDE 1.6.1 / board Nucleo-F746ZG fails during "initializing peripherals" with an Error downloading the following files stem32cube_fw_f7_v1160.zip( HTTP Access Forbidden ) and stm32cube_fw_v1161.zip ( Dependency, not loaded ). This is a 2-3 days old install ... did not have problems with an older install!
2021-07-25 6:43 AM
That seems to be a bigger problem with ST. I wanted to play a bit with TouchGFX 4.17.0. But after the installation no examples and templates are shown. With Wireshark I get the same error message as with CubeMX.
No. Time Source Destination Protocol Length Info
165 5.381589 23.53.43.8 192.***.***.*** HTTP/XML 60 HTTP/1.1 403 Forbidden -> CubeMX
171 5.425317 23.53.43.8 192.***.***.*** HTTP/XML 730 HTTP/1.1 403 Forbidden -> CubeMX
714 47.921601 23.53.43.24 192.***.***.*** HTTP/XML 662 HTTP/1.1 403 Forbidden -> TouchGFX
2021-07-25 11:52 PM
We’re experiencing an outage with all the connections to sw-center. We'll get back to you on this thread once resolved.
2021-07-26 12:23 AM
The outage should now be resolved, please confirm the resolution on your side too.
2021-07-26 12:58 AM
Top! Both CubeMX and TouchGFX now work.
Thanks for the quick solution.
Rolf
2021-07-26 8:05 PM
Working now Thanks,
Some observations -
Anyway after extending the screen look time to 2 hours and removing the S7 1.16.0 then using "Install Now" on S7 1.16.1 , waiting more than 1 hour for 1.16.0 to download (again) and install followed by 1.16.1 to download and install, everting is in order and working !
Regards,
A
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.