2022-01-24 10:33 PM
Hi.
I`m generating a project from stm32cudemx version 6.1.2
The MCU I use is a stm32f407v with my own designed board
The f4 series firmware package version I use is 1.25.2
My project consists of usb msc device only, with sd card connecting through SDIO, DMA enabled, using fatfs library
What I wanna do is to create files through fatfs into the sdcard, and handle these file in windows, while the board is connected to my PC through usb.
I can cut and copy files from\to sdcard, but when I press "delete" in windows, the file icon disappears like it is removed, but when I press refresh, or when I disconnect and connect again the usb, or when I connect the card to pc through a card reader, the deleted file appears again with size of zero.
Can any body tell me whats wrong here?????
2022-01-25 12:33 AM
Also formatting the drive is not possible, gives the error "windows was unable to complete the format"
2022-01-25 12:33 AM
There is no "delete" at sector level. Either your write doesn't work or you don't sync ("eject") the volume before disconnecting it from the host, so the relevant write command is not sent to it from the host.
2022-01-25 3:08 AM
to gbm
Thanks for the answer
how should I do the "sync" from windows?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.