2019-04-18 12:30 AM
Hi,
I am using cube mx FatFS library for Data Logging in a SD card using STM32F401 board.
The examples available on internet, are only writing one time in the text file. I have tried \r and \n in code for new line, But each time I write it starts from line one.
Here is my code
FATFS SD_FATFS;
FIL MyFile;
unsigned int TestByte;
char FilePath[] = "Write1.txt";
char Data[] = "Hello World!";
char Data1[100];
while (1)
{
HAL_Delay(2000);
HAL_GPIO_TogglePin(LED_ORANGE_PORT,LED_ORANGE_PIN);
if(f_open(&MyFile, FilePath, FA_WRITE | FA_CREATE_ALWAYS) != FR_OK)
HAL_GPIO_WritePin(LED_RED_PORT,LED_RED_PIN,GPIO_PIN_SET);
sprintf((char *) Data1,(char *)"\r\n");
if( f_write(&MyFile,Data1,sizeof(Data1),&TestByte) != FR_OK)
HAL_GPIO_WritePin(LED_RED_PORT,LED_RED_PIN,GPIO_PIN_SET);
if(f_write(&MyFile,Data,sizeof(Data),&TestByte) != FR_OK)
HAL_GPIO_WritePin(LED_RED_PORT,LED_RED_PIN,GPIO_PIN_SET);
if(f_close(&MyFile) != FR_OK)
HAL_GPIO_WritePin(LED_RED_PORT,LED_RED_PIN,GPIO_PIN_SET);
}
Please help
Thanks in advance
2019-04-18 1:13 AM
Hi
Don't use FA_CREATE_ALWAYS flag. This flag "Creates a new file. If the file is existing, it will be truncated and overwritten."
Use FA_OPEN_ALWAYS flag to for sequentially write data.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.