2022-10-13 8:47 PM
After the firmware is updated, it gets executed normally. When I want to update the firmware, I send a start or an ampersand to the target board through Terminal program from my PC. My firmware on receipt of this character will enable the WDT and go into an infinite loop allowing the WDT to Reset the controller. This way there is no need to keep changing the jumper and resetting the controller manually while development is going on. This method has been working fine. However, after an update in CubeMX and associated packages for the controllers (stm32f103 and stm32f407), my target boards started resetting immediately after the application firmware is loaded. If I change the Boot0 pin (execute mode) and then apply power the application firmware works ok. This is not happening with old projects/code. How can I resolve this issue which is really bothering? Thank you.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.