cancel
Showing results for 
Search instead for 
Did you mean: 

Has anyone open a Project/Example under STM32_FW_F3 yet.

TFlac
Associate III

I am using STM32CubeMX, STM32CubeIDE and val board STM32F303RE. All I wish to do is recreate the project/examples with the firmware package using CUBEMX and CUBE_IDE combo.

I have been able to get the Examples to work but not as the documents explain.

What I do to get the example design "TIMPWMInput" to work. I open STM32CubeIDE under CubeMX assistance, select a board and instruct the tools not to configure peripherals. This give me the project file structure.

Next, I go to the folder with the STM32_FW_F3 and open the SRC/INC files within the TIMPWNInput. I simply CUT and PASTE the code right over top the code that CUBEMX created. I literally erase everything the CubeMX created. The design now works.

This is not the way it should work as if I update the design via CubeMX it will overwrite everything I pasted providing I keep the items within the USER-BRACKETS which I do.

I wish to create the design 100% through CubeMX to look just like the example code. This should not be that hard to do. I'm very close using CubeMX as I get no BUILD errors. It downloads fine via DEBUG.

It halts at HAL_INIT as it should, I run the design and nothing comes out through "Live Expression"

Any help would be super!

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.