2025-08-04 12:14 PM
Hi! I'm working on setting up FDCAN communication using the STM32N6570X0-Q Nucleo Board. However, when I try to modify the bit timing parameters—such as the Nominal Prescaler, Nominal Time Seg1, or Seg2—the baud rate doesn't seem to change regardless of the values I set.
On the receiving side, I'm using a STM32H533RE Nucleo Board to echo the messages, but it doesn't receive anything—so I suspect the issue may be with the timing configuration on the N6570X0-Q.
Do you have any idea what might be causing this behavior?
Thanks in advance!
Solved! Go to Solution.
2025-08-05 8:18 AM
Hello @guillerminaborrazas,
Thank you for bringing this issue to our attention.
Issue has been escalated to dev team for resolution under this internal ticket 215362.
I will keep you posted with updates.
Thanks.
Mahmoud
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-08-05 7:07 AM
Hello @guillerminaborrazas ,
First let me thank you for posting and welcome to the ST Community.
Your request is under investigation, and I will get back to you ASAP.
Thanks.
Mahmoud
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-08-05 8:18 AM
Hello @guillerminaborrazas,
Thank you for bringing this issue to our attention.
Issue has been escalated to dev team for resolution under this internal ticket 215362.
I will keep you posted with updates.
Thanks.
Mahmoud
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-08-05 8:43 AM
@Mahmoud Ben Romdhane thank you for your quick response.
From what I’ve seen using an oscilloscope, the messages are indeed being sent at 1 kbit/s.
Hope the issue is resolved.
Guillermina
2025-08-18 7:48 AM
Hi! @Mahmoud Ben Romdhane is there any news on this subject? Thank you!
2025-08-18 8:45 AM
Hello @guillerminaborrazas ,
I will keep you informed as soon as this issue is resolved.
Thanks.
Mahmoud
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-11-10 5:20 AM
I'm experiencing similar issues. Any news on this?
2026-05-02 1:53 PM
Hi,
I had the same problem described by @guillerminaborrazas in the configuration panel of CubeMX: even if I would set the correct bit timing parameters (double checked and properly working on a different NUCLEO board), the CAN bus was off (REC and TEC increasing at each and every in/out message and LEC register showing any sort of error code).
I had been struggling for a month now, then I updated CubeMX to the latest available version (6.17.0) and the problem got solved: the configuration panel is working properly, as the communication is.
Would this be useful to some of you guys, I attach a CubeIDE project of a standard CAN network which is currently working on my NUCLEO-N657X0 both in Tx and in Rx (tested with a PCAN hardware).
If somebody needs help in the configuration please just ask :)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.