2021-08-27 2:55 AM
When I try (as stated in the CubeMX handbook Section 3.3.2)
cd "C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeMX\"
java.exe -jar STM32CubeMX.exe -ior
java -jar "C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeMX\STM32CubeMX.exe" -q cubeMxGeneratewith cubeMXGenerate just containing
config load myconfig.iocthe GUI comes up all the time.
I would expect that the command-line mode would work without a GUI and thus can be run on a CI server for example. Is that a known issue to be fixed?
2021-08-27 5:23 AM
Hello @FS.1 ,
Thank you for your post,
I'll check the point and I'll get back to you.
Khouloud
2021-08-27 5:53 AM
Hi again @FS.1 ,
I have checked from my side using the latest CubeMX version (6.3.0) and I cannot reproduce the issue.
Could you please switch to the latest release and tell me if it works fine for your or not?
Otherwise, could you please give me more details about your machine and share the script used with your ioc file?
Thanks, Khouloud
2021-08-27 6:26 AM
Hi,
thanks for testing.
I just upgraded to 6.3.0 and
java -jar "C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeMX\STM32CubeMX.exe" -istarts CubeMX GUI in version 6.3.0.
No interactive console.
Java ist the following:
> java --version
openjdk 11.0.11 2021-04-20
OpenJDK Runtime Environment AdoptOpenJDK-11.0.11+9 (build 11.0.11+9)
OpenJDK 64-Bit Server VM AdoptOpenJDK-11.0.11+9 (build 11.0.11+9, mixed mode)
2021-08-27 6:33 AM
Hello @FS.1
Please use the following command :
C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeMX>jre\bin\java.exe -jar STM32CubeMX.exe -q your_scriptThanks, Khouloud
2021-08-31 1:51 AM
Hi,
running
PS C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeMX> .\jre\bin\java.exe -jar STM32CubeMX.exe -ijust runs CubeMX UI and not the interactive command-line as stated in the handbook.
Running
PS C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeMX> .\jre\bin\java.exe -jar STM32CubeMX.exe -q C:\path\to\project\cubeMxGeneratedoes not work because the IOC file lies in C:\path\to\project\ just like the script I want to run.
Running
PS C:\C:\path\to\project> & 'C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeMX\jre\bin\java.exe' -jar 'C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeMX\STM32CubeMX.exe' -q .\cubeMxGeneratekind of works but still shows a "created with an older version, what do you want to do?" window.
Is it possible to do the "continue" or "migrate" automatically?
Also, the command ends with OK but apparently does not return and has to be finished with Ctrl+C ... so it cannot be run automatically from another script or a CI system.
As it stands now, CubeMX is not ready for CI business. In command-line oder script mode it should never open any windows.
Cheers
2021-08-31 2:10 AM
Also, running
swmgr refresh
swmgr install stm32cube_f4_1.5.0 askwithin the script opens a progress bar window and while the package is installed, the MainUpdater times out 15 times and then gives up.
Command-line mode is completely untested and unusable. :(
Cheers
2022-01-13 2:26 AM
Any update on this? I'd like to use this feature as well but am having the same issue. I'm testing on version 6.3.0.
2022-01-23 3:17 AM
Anyone...?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.