2018-12-22 9:22 AM
Hi,
Looking at the block diagram in the datasheet, ABH1, AHB2, AHB3, AHB4, AXI are listed as supporting 200MHz.
Cube (v5.0.0, H7 v1.3.0) however will not allow them to be set higher than 100 MHz, and says the must be <- 100MHz in the hover text.
Is cube or the datasheet correct?
Thanks,
Jacob
Solved! Go to Solution.
2018-12-22 9:30 AM
Nevermind, didn't realize they need to be 1/2 the core speed. It lets me do 200MHz if the core is 400 MHz.
Everything is fine : )
2018-12-22 9:30 AM
Nevermind, didn't realize they need to be 1/2 the core speed. It lets me do 200MHz if the core is 400 MHz.
Everything is fine : )
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.