2019-12-11 11:38 AM
Minor bug, but it threw me off for a bit. When selecting ETH for the STM32H750, in the Parameter Settings there is a warning that ETH can only work with address 0x2400_0000. That is actually D1 SRAM which is not accessible by the Ethernet MAC, it needs to be D2 SRAM. The actual settings below (0x3004_0000) are correct, but the warning is incorrect.
I don't have Ethernet working yet, but hopefully soon...
will
2019-12-11 12:03 PM
...and forgot to also mention that those RAM settings get ignored anyway with Atollic/CubeIDE. For Kiel/IAR the generated code puts those buffers in the designated areas, but for Atollic/CubeIDE it just creates the data structures without any location overrides, so they get thrown in the default area which is DTCM.
will
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.